5/26/2021 1:09 AM | |
Joined: 11/16/2016 Last visit: 11/20/2024 Posts: 45 Rating:
|
Hello, Please, how do I use wipeout for s7-200? and is it possible for windows 7? Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/26/2021 07:16:50New subject after splitting |
|
5/26/2021 1:18 AM | |
Joined: 3/9/2018 Last visit: 9/3/2025 Posts: 208 Rating:
|
|
Last edited by: Henry1675 at: 05/26/2021 17:05:45 |
|
5/26/2021 8:48 AM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
Hello, Please check this FAQ: Resetting the S7-200 to the factory default settings (WIPEOUT) Please note WIPOUT is a toll to reset S7-200 CPU to factory setting even if it's password protected. After using it, there will be no chance to retrieve the software that was stored on the CPU. |
Ayman Elotaify |
|
5/29/2021 7:13 AM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
Hi, To communicate with S7-200 CPU using PC adapter USB "xxxxx- 0CB20", please follow steps here: Which configuration do you need for "PC Adapter USB" in conjunction with MicroWin and S7-200? |
Ayman Elotaify |
|
5/29/2021 11:25 AM | |
Joined: 11/16/2016 Last visit: 11/20/2024 Posts: 45 Rating:
|
Thank you but I not have any problem with this because I communicate with same pc adapter to another cpu so i think that the cpu is faulty but to be sure I would use wipeout to try if the cpu work or not. |
5/29/2021 11:43 AM | |
Joined: 9/21/2012 Last visit: 9/10/2025 Posts: 4708 Rating:
|
If you can't connect to the CPU, then you can't do a wipeout either... |
5/30/2021 4:51 PM | |
Joined: 11/16/2016 Last visit: 11/20/2024 Posts: 45 Rating:
|
so the PLC is Faulty? |
5/30/2021 11:28 PM | |
Joined: 3/9/2018 Last visit: 9/3/2025 Posts: 208 Rating:
|
If you power up the plc in stop mode the SF LED is on? |
5/31/2021 9:51 AM | |
Joined: 11/16/2016 Last visit: 11/20/2024 Posts: 45 Rating:
|
yes |
5/31/2021 9:54 AM | |
Joined: 11/16/2016 Last visit: 11/20/2024 Posts: 45 Rating:
|
I Tried wipeout but I can't use it on windows 7 64bits it need 32bits, there is one which work with 62 bits? |
Follow us on