11/2/2022 11:39 AM | |
Joined: 10/5/2022 Last visit: 12/16/2024 Posts: 4 Rating:
|
Is LWE V1.1.1 available as a standalone download? I can only see it as a LSC V8.3 SP1 bundle. Thanks |
11/2/2022 12:28 PM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35963 Rating:
|
I don't think that it is a firmware issue. Firmware update V1.83.02 for LOGO! 8.3 basic devicesMy opinion is the installation of LWE is not correct because the transfer window doesn't show a interface. You can start a Support Request to ask Siemens directly. |
4/26/2024 1:01 PM | |
Joined: 4/26/2024 Last visit: 7/15/2025 Posts: 2 Rating:
|
Did you solve the problem?I have the same problem and have tried everything.Thank you |