9/15/2014 1:12 PM | |
Joined: 12/1/2009 Last visit: 7/14/2025 Posts: 672 Rating:
|
Dear All, as requested by other forum members here aModbus RTU SlaveCommunication function block. The following SIMATIC S7 communication processor issupported:
GENERAL INFORMATION & SUPPORT For installation, connection and interface configuration of your communication processor module kindly follow its respective documentation. I also advise you to take some time and go through the general information about Modbus provided by our forum member smiffy. Especially if you are a beginner in Modbus, seek for support or just want to learn more about it. I hope tomake your life a bit easier with this development.
With Best Regards SEEKING FOR CP341TO DEVELOP DRIVER FOR CP341 DRIVER DOWNLOAD (ATTACHMENTS) The attached program files need to be retrieved within the SIMATIC Manager. Currently there is only one manualfor theCP340version but the others are all working in the same way just with different function blocks. MBSL340.PDF - Manual for Modbus RTU Master for CP340 MBSL340.ZIP -Example projectfor Modbus RTU Slavedriver for CP340 MANUAL MBSL340 AttachmentMBSL340 V100.pdf (4045 Downloads) |
Last edited by: TIBI68 at: 9/15/2014 1:29 PMGive us your feedback and show us your respect! |
|
This contribution was helpful to
47 thankful Users
|
9/15/2014 1:14 PM | |
Joined: 12/1/2009 Last visit: 7/14/2025 Posts: 672 Rating:
|
MBSL340 Thanks for downloading ! Some feedback anda click onthe "Thanks" button would be appreciated. AttachmentMBSL340.zip (3317 Downloads) |
Last edited by: TIBI68 at: 9/24/2014 9:53 AMGive us your feedback and show us your respect! |
|
This contribution was helpful to
51 thankful Users
|
9/27/2014 9:14 PM | |
Posts: 2 Rating:
|
thanks dude. |
This contribution was helpful to
3 thankful Users |
10/3/2014 1:35 PM | |
Posts: 168 Rating:
|
Great job, thanks for sharing |
This contribution was helpful to
1 thankful Users |
10/29/2014 4:09 PM | |
Joined: 12/1/2009 Last visit: 7/14/2025 Posts: 672 Rating:
|
Dear Hopling, I can make the block for CP341 in no time but I dont have the CP for testing it. Best Regards. |
Give us your feedback and show us your respect! |
|
10/30/2014 8:03 AM | |
Joined: 12/1/2009 Last visit: 7/14/2025 Posts: 672 Rating:
|
Dear Hopling, when it communicates it will work for the full functionality. Onlythe calls of the standard function blocks will change, the rest of the code will be the same. I make the changes and will send you the beta to your email for testing. Gve me some time for that changes while I am a bit busy at the moment. Best Regards. |
Give us your feedback and show us your respect! |
|
Follow us on