11/19/2009 5:36 PM | |
Joined: 1/18/2007 Last visit: 8/20/2015 Posts: 16 Rating:
|
Also, I dont think you need a dedicated CP. I/O driver with standard ethernet port on the SCADA PC will work fine. |
11/20/2009 10:30 AM | |
Posts: 6 Rating:
|
Hi Farlo, many thanks for that Richard |
3/18/2010 4:37 PM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
Hi, The FAQ “How can you establish a connection between a S7-1200 PLC and SIMATIC NET OPC?” http://support.automation.siemens.com/BR/view/en/39960679(Intranet) shows how to communicate with SIMATIC NET OPC. The FAQ Flexible Decoding and Processing of Data Matrix Codes with S7-1200http://support.automation.siemens.com/BR/view/en/40603943 shows how PC Access could also be used. Despite of not 100% homologate, they work with some restrictions. The tip is to program a S7-300/400 connection and gives rack=0 and slot=1. |
Denilson Pegaia |
|
This contribution was helpful to
2 thankful Users |
5/1/2014 11:29 AM | |
Posts: 12 Rating:
|
hi Farlo! can you give me ebook to config it! I'm really have problemwith connect S7-1200 in TIA PORTAL to intouchwonderware |
7/1/2014 11:22 PM | |
Posts: 16 Rating:
|
Using the S7CP_200 seems to apply to an S7300 configured with TIA Portal (v11) also. |
9/4/2014 10:09 AM | |
Posts: 43 Rating:
|
I succeded to connect into Wonderware using Net2PLC.. |
This contribution was helpful to
1 thankful Users |
12/24/2014 2:21 PM | |
Joined: 12/4/2013 Last visit: 9/8/2025 Posts: 6 Rating:
|
Hi All, Got this working myself this morning. After many headaches. Used the DASSIDirect V3.0 driver. Was very difficult to setup. The WWClient application was very helpful, you can download from Wonderware when you download the driver. Nothing seemed to work until i ran the WWClient, but i think that is because i had the wrong addesses selected. I have made a small word document detailing my config. IP address are for test system.
AttachmentS71200 to Touch Dev01.zip (2716 Downloads) |
This contribution was helpful to
3 thankful Users |
6/24/2020 12:34 PM | |
Joined: 8/11/2018 Last visit: 7/22/2024 Posts: 15 Rating:
|
hi |
Last edited by: Jen_Moderator at: 06/24/2020 13:38:55Embedded video. |
|
7/8/2020 9:05 AM | |
Joined: 10/14/2015 Last visit: 11/28/2024 Posts: 2 Rating:
|
Hello, Can you please share again what you did to connect to a s1500 plc. |
Follow us on