2/23/2022 3:03 PM | |
Joined: 9/27/2006 Last visit: 9/14/2025 Posts: 12408 Rating:
|
Hello; The link provided by Bjorarkor allow you to download only the latest SP8 and SP9 for Microwin v4.0. To install these, you need a valid license for Microwin v4.0, 6ES7810-2CC03-0YX0. Even though this part number is considered obslolete, it is still availabe from the Siemens Idustry Mall (electronic catalog), so ask your nearest Siemens rep. to find out about pricing and availability. https://mall.industry.siemens.com/mall/en/b1/Catalog/Product/6ES7810-2CC03-0YX0 Then install SP9 from the previous link. Note that Microwin v4.0 SP9 is only compatible up to Win 7 64-bits. It will install on Windows 10, but the drivers to connect to a S7-200 CPU will not work This is a proposed solution: You can download a trial version (at no cost, working for 21 days) of Step 7 v5.6 SP2 through this link: https://support.industry.siemens.com/cs/ww/en/view/109773842 Install Step 7 v5.6 SP2 under Windows 10, along with Microwin v4.0 SP9, and then the complete funtionnality of Microwin will be available. Hope this helps Daniel Chartier |
Follow us on