5/22/2022 7:02 PM | |
Joined: 10/22/2011 Last visit: 8/28/2025 Posts: 308 Rating:
|
Dear All, CPU414-2 is installed on a machine with 3 Control Techniques drives and 1 ET200 station connected via Profibus problem is that during normal running, suddenly PLC trips on BUS2 fault for instantly (for a second) and goes. due to this trip, control techniques drives goes to trip and hence machine stops I am unable to detect the node causing this situation as fault comes instantly and goes is there any way to find out the faulty node? Diagnostic buffer is also attached Thanks AttachmentDiagnose.txt (805 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on