5/27/2006 7:15 AM | |
Posts: 3149 Rating:
|
Hi, copy your installation-CD to your harddrive and then start the installation.. http://support.automation.siemens.com/WW/view/en/22057394 good luck, nemo |
5/27/2006 9:10 AM | |
Posts: 11 Rating:
|
Update,
Hi Nemo,
I downloaded again just in case and in put the SP1 update on to C: drive to see if the "from" drive made any difference. previously it was from a network drive.
Still the same.
Tried setup from unzipped directory, then inside CD_1 no difference.
Attached are screen shots showing problem.
Setup_1 shows that the normal path below the Target directory is missing.
Setup_2 shows that when you scroll down the browse button dissappears.
Setup_3 shows when you go back to SP1 selection the browse button stays missing.
DC
Attachmentsetup_1.zip (506 Downloads) |
Last edited by: DC at: 5/27/2006 9:18 AM |
|
Follow us on