6/9/2022 10:02 AM | |
Posts: 34 Rating:
|
Hello I am still waiting for the hardware but want to simulate it and program the control flow. What is not clear for me is how to communicate (acknowledge) to the camera that the code is received, and that it should publish the second code (2 codes in my application). In the end I would expect to send acknowledge again to state that all current codes are received. Document to OIDCyclic says: 2.3.2 Start the trigger HW_ID_USERDATA Input HW_SUBMODULE Hardware ID of the module "User data" PROGRAM Input Byte Program number 1-15 Note: In the event of a program change, the DISA bit must be set. DISA Input Bool Disable: Disable manual control in the WBM IN_OP Output Bool In operation: 0 = Error message is displayed, 1 = Device functioning, no error RDY Output Bool Ready: 0 = Device startup or device in Stop, 1 = Device in processing mode (Run) ERROR Output Bool Error: 1 = An error has occurred. PROGRAM_OUT Output Byte Number of the program currently selected on the reader |
Last edited by: tystnariluren at: 06/09/2022 10:03:10 |
|
6/9/2022 10:27 AM | |
Joined: 10/19/2017 Last visit: 9/12/2025 Posts: 9 Rating:
|
Hello, there is no acknowledgement. The new result comes automatically and overwrites the old result. |
Follow us on