(0)| 5/25/2023 11:05 AM | |
|
Joined: 1/21/2013 Last visit: 1/23/2026 Posts: 4430 Rating:
|
Hi Paul, Although I am not quite sure, Fast Start-up (FSU) as defined in the PROFINET standard should be covered by the prioritized startup feature. The list of devices that support this and other features can be found in the FAQ "Which IO controllers and IO devices support the following functions in STEP 7 (TIA Portal): IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, MSI/MSO, I device, clock-synchronized mode, system redundancy and option handling?". More information about prioritized startup can be found in the function manual "SIMATIC PROFINET PROFINET with STEP 7". Kind regards |
This contribution was helpful to
|
|
| 5/25/2023 11:29 AM | |
|
Posts: 12 Rating:
|
Thank you Stefan, That's what I was looking for. Regards, |
Follow us on