7/13/2023 2:22 PM | |
Posts: 6 Rating:
|
HI, I have a problem in restoring the operating system on IPC227E. I created a bootable usb key using the iem-os-1.5.2-4-amd64-install.iso file but the result is always the same, that is, negative. I am having the security lockout problem for the security policies when doing a restore via usb I'm trying to reinstall the iem-os-1.5.2-4-amd64-install file but I can't. I checked in the bios if I could disable secure boot but there is no option. I updated the bios to the latest version, but there is no option to disable secure boot. When I bought it there was no dvd or anything to restore but on the boot screen I was seeing this. Now I want to reset the IED OS system ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/14/2023 08:28:17New subject after splitting |
|
7/13/2023 2:30 PM | |
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi,
this is the product conference for the IOT2040/IOT2050. Please open a topic in the Industrial Edge product conference for this. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to
1 thankful Users |
7/13/2023 2:56 PM | |
Posts: 6 Rating:
|
Ok, this is a new Topic. Thank you. |
This contribution was helpful to
1 thankful Users |
7/14/2023 8:28 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject Info about how to restore IEM OS in IPC227E is published within the conference Industrial Edge. Jen_Moderator |
Follow us on