6/22/2023 10:06 AM | |
Joined: 10/20/2015 Last visit: 6/10/2025 Posts: 12 Rating:
|
Good morning, I have the same problem: i am using siemens tablet itp1000, i have SmartClient but when i connect to the panel with the SmartServer i can only browse the pages but no INPUT, no keyboard comes out. Do I have to install WinCC flexible 2008 SP5 Runtime Trial?. At the moment I can't install it because the tablet is not ours and they haven't blocked installations from Windows. Is there any other way to bring up the keyboard? Thanks, Giulio ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/23/2023 05:51:21New subject after splitting Last edited by: Jen_Moderator at: 06/23/2023 05:54:22Spelling mistake in the headline corrected . |
|
Follow us on