9/4/2023 12:49 PM | |
Joined: 9/15/2015 Last visit: 6/21/2025 Posts: 4 Rating:
|
Hello Umencho, Can you refresh link to "Communications" (it seams that the link is broken) where I assume is a procedure to upload from COROS OP5 with COMTEXT. For the OP, I am not sure if it was made with COMTEXT or with Protool but I would like to try it with COMTEXT which intuitively, I am not able to get into procedure of how to upload. Firmware of the OP5-A1 is V1.30/1, maybe that can tell something? After I installed a COMTEXT, I got two "warning" messages like on the screen in attachment. I tried with few different copies of sw and the result is the same, but from that screen I am not able to find any option to do transfer. Btw, I am using old laptop with Windows XP installed. Can that be a problem? Maybe COMTEXT needs plain DOS OS to work properly? Maybe a link to user manual for COMTEXT v3.1? In case the source was made with Protool, do you maybe know what sw to use for Backup/Restore? Thank you! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/28/2023 13:03:55New subject after splitting |
|
Follow us on