9/13/2015 3:40 AM | |
Joined: 10/12/2014 Last visit: 3/17/2025 Posts: 66 Rating:
|
sir ; i m from sri lanka . Here i attached the error code image which is appeared in the Simatic panel, simatic panel-c7 633 p error code ($551 as address 2 not possible ) .In simatic panel stop also blinking . In this situation when I try to download the backup program , I cant proceed ,because when downloading the program using simatic manager it gives another error.Here i also attached the simatic manager error code image which appeared in the program. sir please help me to overcome with this fault. Attachmenterror.zip (1798 Downloads) |
Last edited by: neththi at: 9/13/2015 4:18:37 AMLast edited by: neththi at: 9/13/2015 4:29:51 AM |
|
9/13/2015 6:45 AM | |
Joined: 12/18/2014 Last visit: 9/16/2025 Posts: 35964 Rating:
|
In the manaul you can read: system message 551: Remedy: Check MPI Station and wiring. The Manual you can load here: |
2/21/2017 10:53 PM | |
Posts: 2 Rating:
|
You probably solved it. Anyway if the Programe is lost then you have to download through RS-232. |
7/16/2018 7:34 AM | |
Joined: 7/14/2018 Last visit: 11/27/2024 Posts: 2 Rating:
|
do you use RS 232 communication cable and try it in prosave |
10/25/2023 8:43 AM | |
Posts: 3 Rating:
|
please reload program. and restore from simantic manager it will solve |
Follow us on