11/28/2023 3:13 PM | |
Joined: 4/7/2022 Last visit: 4/2/2025 Posts: 1 Rating:
|
Hello Arve, Did you find the solution ? I'm in the same case as yours. Best Regards, Benoît ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 11/28/2023 15:20:31Quote added Last edited by: The Helping Hand at: 11/28/2023 15:21:09New subject after splitting |
|
11/28/2023 3:46 PM | |
Joined: 7/19/2022 Last visit: 9/10/2025 Posts: 436 Rating:
|
HelloBEN21700, If you see error "1619" during installation, this could be caused by the Windows installer. So, take a look at these FAQs: Also tell you that even if you have migrated the project from SP3 to SP5, check the version of the device that you have configured in the project because, at least in TIA Portal, the project is migrated but not the version. You would have to do this manually |
Last edited by: JBS98 at: 11/28/2023 15:50:02If this Information really helps, you could use the Rate function |
|
11/29/2023 11:59 AM | |
Joined: 8/3/2009 Last visit: 9/10/2025 Posts: 16386 Rating:
|
Hello BEN21700 Install the latest Upd for Engineering and Runtime: https://support.industry.siemens.com/cs/de/en/view/109757233 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on