2/22/2023 3:47 PM | |
Joined: 5/30/2022 Last visit: 9/17/2025 Posts: 634 Rating:
|
Hi daercole, A coupling of panels from Protool to an S71500 CPU configured in TIA Portal is an unusual combination for which, as seen above, no general recommendation or function guarantee can be given. The only thing that could work would be to use the old S7300/400 communication channel and allow communication in the S71500 with Put/Get and work with absolute DBs. But even for this combination, we cannot guarantee the functionality of these old panels. The following FAQ describes a similar constellation, but with WinCC flexible. For Protool, we have no experience here, as the product has been discontinued for some time: How do you access S7-1200 tags with a panel or RT configured with WinCC flexible 2008 SP2? |
If this information really helps, you could use the Rate function. |
|
Follow us on