6/20/2013 6:00 PM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, Have a look at: Why is the installation aborted after 68% during the "Registering application" action? If that does not solve your problem, please return and mention your OS, version of step&, firmware version of the adapter. Regards, Marcjan |
Problem solved? |
|
6/24/2013 5:05 PM | |
Joined: 11/23/2011 Last visit: 9/3/2025 Posts: 202 Rating:
|
Hello N.Vijay, please have a look on the following FAQ. Maybe it would be helpful: http://support.automation.siemens.com/WW/view/en/37855423 Greetings, KM_AS |
11/25/2014 9:29 AM | |
Posts: 30 Rating:
|
Dear I am facing unexpected problem! First ! My Laptop Hardware & Software Specifications Dell Inspiron 1564 OS: Windows7 (64-bit) SIMATIC S7 V5.5 SP1 Second ! Plz have a look at files in attached .zip folder Attached zip file contains 3 pics 1-Snapshot of my USB to MPI Adapter 6ES7 972-OCB20-OXA0 PC Adapter V5.4 2-Snapshot of error about drivers detail before installing PC Adapter drivers downloaded from https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=27062840 &caller=view 3- Snapshot of message about drivers detail after installing drivers downloaded from above link. Now putting forward my problem ! Although downloaded drivers are successfully installed on my system. The problem is that readme file doesn't contain information about drivers support for 64-bit system. Moreover ! Order Entry of hardware for which drivers should support, is same as that of printed on my own PCI adapter but the manual contains different infromation about PCI adapter of the same Order entry ID. For example My PCI adapter contins only two LEDs (1- Power , 2- Active) while information in the manual describe different number of LEDs. Whenever I try to communicate with PLC, Error message appear "Communication Link to Adapter damaged". Help me to resolve this problem Attachmentpics.zip (1275 Downloads) |
2/7/2024 9:24 AM | |
Posts: 5 Rating:
|
Hy Hello, I have a small problem with the connection between the PLC S7 300 and the PC and I would like to know how I can download the pilot? |
Follow us on