9/4/2024 8:28 AM | |
Joined: 1/16/2021 Last visit: 11/30/2024 Posts: 1 Rating:
|
Has anyone solved the problem yet? |
9/4/2024 12:02 PM | |
Joined: 12/18/2014 Last visit: 9/13/2025 Posts: 35957 Rating:
|
No, there is no solution yet. Siemens has not taken a firmware update to solve this problem ... |
10/27/2024 8:27 AM | |
Joined: 12/18/2014 Last visit: 9/13/2025 Posts: 35957 Rating:
|
The problem "LOGO! 8.4 slave does not start after power failure" was solved with the firmware update to V1.84.03. I upgraded the firmware and tested it, and the error was fixed. You can download the soft- and firmware update from here: Firmware update for LOGO! 8.4 basic devices and service pack 1 for LOGO! Soft Comfort V8.4 |
This contribution was helpful to
2 thankful Users |
Follow us on