11/20/2024 1:17 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, Yes, that could make your CPU to STOP. (Your program reads and write to missing Profinet IO device) You can use Error OB's, it might help to let the CPU in Run, see the following link: Which organization blocks can you use in STEP 7 (TIA Portal)? Best regards, Wizard |
11/21/2024 8:25 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, In that case there should be some programming. You can decouple a profinet IO device, but in your program there should be some pre conditioning. Not to read and write to that device etc. Perhaps the following link might help. How do you switch off (decouple) a slave without causing an error entry to appear in OB 86/OB 122? Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
Follow us on