12/11/2024 9:09 AM | |
Joined: 2/12/2024 Last visit: 12/26/2024 Posts: 2 Rating:
|
Hi, Logo module 6ED1052-1CC08-0BA2 firmware 1.84.03 LogoSoftComfort V8.4.1 After i type in the IP adress of Logo Base module in a brower, the url changes into 192.168.1.47/logo_variable_01.shtm and i get not found on this page, and i do not know why. I have the same problem on another identical logo. I loaded also an LWE project on the SD card. Access to the customised site is OK On Logo BM online settings LSC and LWE Access Password is enabled Webserver access HTTP is enabled Web user is enabled TDE access enabled (Some issue with this option diabled) I used an 4GB SD card formated in Fat32 Can anyone point me into the wright direction to solve the webserver access towards logo BM Best regards, Fabrizio AttachmentLogo-BM-Webserver-Access.pdf (182 Downloads) |
12/11/2024 1:09 PM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35960 Rating:
|
Clear your browser cache. |
Follow us on