(0)| 5/31/2024 4:10 AM | |
|
Joined: 1/7/2022 Last visit: 9/11/2025 Posts: 2 Rating:
|
Did this problem occur again in the mean time? I have a USB stick with ample storage (Sandisk, USB3.0, 120GB) and It's logging alright for the first hours (2-3hours) but after that the trending page is not able to retrieve the values from the logged files, it gives '###' as proces value from the datapoint. Also the noteble thing is that my log files for some reason are all 36KB "when they stop logging". any experience with this by any chance? Thanks in advance! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/31/2024 04:12:42New subject after splitting |
|
| 1/9/2025 7:59 AM | |
|
Joined: 8/3/2009 Last visit: 1/9/2026 Posts: 16629 Rating:
|
Hello BenjaminBrns first of all what do you mean with large amount of data... If you have a Comfort Panel you can only store limited data: https://support.industry.siemens.com/cs/ww/en/view/109815056/149280625163 So you should not use more data than 20000 Entries per log. So a 2GB Memory should last very long. Also Backup Files of the Panel are only a few MB and no GB. This kind of Panels are not made for storing historical data of a huge amount. You can also use the suggested external memory devices from Siemens (SD and USB) this should work in any case. Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on