(0)| 1/10/2025 7:31 AM | |
|
Joined: 6/10/2022 Last visit: 9/8/2025 Posts: 3 Rating:
|
Hello guys , we have a problem with updating OS on TP1200 Comfort HMI. We need update OS to version 14 or higher. We tried OS version 14 and 17. Update was OK bud ethernet connection with OS greather than 13 is not alive . Ethernet adapter gets IP 0.0.0.0 and we are not able to write IP adress to ethernet and also we are not able to connect with ethernet to the HMI panel. We tried everithing to get it alive but without success. We made changes with Transfer settings ( Automatic, Manual , PN/IE , Ethernet ) , we also made changes with IP settings ( DHCP , Static IP ) . But nothing helped to get ethernet ports alive. After restore from USB ( OS13 image ) ethernet connection is again alive. Can we get some advice ? Screens from panel are attached in the .zip file. AttachmentTP1200 screens.zip (246 Downloads) |
| 1/13/2025 7:35 AM | |
|
Joined: 4/24/2006 Last visit: 1/15/2026 Posts: 9105 Rating:
|
Hi, I think the only option would be to send panel to Repair center. Best regards, Wizard |
| 1/14/2025 9:49 AM | |
|
Joined: 6/10/2022 Last visit: 9/8/2025 Posts: 3 Rating:
|
Thank's for the answer. We gave up with that update and HMI will continue with OS13. |
Follow us on