(0)| 1/27/2025 5:46 AM | |
|
Joined: 1/26/2025 Last visit: 1/31/2025 Posts: 4 Rating:
|
The ktp 600 system crashed How do I make a backup? |
| 1/27/2025 8:09 AM | |
|
Joined: 2/17/2020 Last visit: 1/7/2026 Posts: 1251 Rating:
|
Hi, Since you have a Basic Panel, you have two options for backup: USB Recovery (Reset to factory) Mode for 2nd Generation Basic Panels KTP600 model is not indicated as supported by the USB Recovery Mode FAQ, but I would give it a try anyway. If the current state of the panel prevents getting the backup, then you may need to send the unit to Siemens Repair Service. |
|
A rating will be well appreciated. |
|
| 1/27/2025 8:17 AM | |
|
Joined: 4/24/2006 Last visit: 1/8/2026 Posts: 9104 Rating:
|
Hi, In addition to previous answer. Here is a link to manual: SIMATIC HMI HMI devices Basic Panels See chapter 6.5 for more information about Backup Best regards, Wizard |
| 1/27/2025 12:28 PM | |
|
Joined: 1/26/2025 Last visit: 1/31/2025 Posts: 4 Rating:
|
Then I will lose the program for the machine |
| 1/27/2025 7:09 PM | |
|
Joined: 1/26/2025 Last visit: 1/31/2025 Posts: 4 Rating:
|
I can't assign an ip address in the tia portal. The panel is detected without an ip address |
Follow us on