2/12/2025 12:54 PM | |
Joined: 8/5/2022 Last visit: 9/15/2025 Posts: 14 Rating:
|
Hi, A customer of ours have a 1511C-1 PN commisioned by us, and it's been running for a year and a half now, but this morning it went into STOP, then showed a serious firmware exception, restarted a few times and had its memory reset. All DB values were set to start values. According to maintenance personnel, no one was in the vincinity of this CPU at the time of error. It had to be manually set to RUN again. We're not sure what could cause this, maybe fluctuations on the 24V DC? Scary that the CPU wiped itself during this, and weird to see the diagnostics say the first STOP and the memory reset was initiated from the panel. Any ideas of what could cause this?
Attachment12.02. Diagsostics.txt (144 Downloads) |
Last edited by: ostlar at: 02/12/2025 12:56:58Last edited by: Moderator_Lan at: 02/12/2025 13:20:45Code attached |
|
Follow us on