2/13/2025 12:03 PM | |
Joined: 2/17/2020 Last visit: 9/11/2025 Posts: 1251 Rating:
|
Hi, Evaluation of the current mode of the S7-CPU can be performed via the system function "GetPLCMode". Please see: How do you evaluate the "RUN / STOP" mode of the CPU via an HMI operator panel? Then, from the other PLC you can send a signal to the HMI to use the system function "SetPLCMode" to change the S7-CPU mode: As the ET200SP CPU internally is like an S7-1500, I guess this should work. |
A rating will be well appreciated. |
|
Follow us on