4/11/2025 8:31 PM | |
Joined: 1/21/2013 Last visit: 8/29/2025 Posts: 4087 Rating:
|
Hi, According to your screenshot, it somehow looks like Windows App Runtime is installed in an older version, but also in the required version, causing the installation of the required version to fail. Running these commands with Windows PowerShell might provide more information that you can use to manually remove or install a required package.
However, this might cause another application to stop running. So it might work, but most likely the HMI Panel Image Updater will not be installed. So you might consider reporting the problem to Technical Support. Kind regards |
Follow us on