6/8/2025 8:26 AM | |
Joined: 3/24/2025 Last visit: 6/24/2025 Posts: 8 Rating:
|
Hi,
However, when I set a value in the desired field, the LOGO! only applies it if I first stop the device and then start it again (STOP → RUN). I'm using an analog output mark (e.g. AM..4:41-1) that is not connected on the left side in the LOGO! program, so it should be writable via AWS according to this post :Forum Community - Siemens SiePortal ****** 1. While LOGO! is in RUN mode: *********** { ******** 2. While LOGO! is in STOP mode: ********* { ******* 3. After switching back to RUN mode: ***** { " Questions:
I’ve searched extensively through documentation, forums, and example projects, but haven’t found any clear explanation or solution. Still, it’s hard to believe this functionality wouldn’t be supported — it seems like a basic expectation for any IoT-enabled device. Any insights or suggestions would be greatly appreciated. Thank you! Happy to hear your thoughts. |
Last edited by: PierHB at: 06/08/2025 14:39:59 |
|
6/12/2025 3:30 PM | |
Joined: 3/24/2025 Last visit: 6/24/2025 Posts: 8 Rating:
|
Please note: The issue has not been resolved with update V1.83.02. |
Follow us on