7/2/2025 12:56 PM | |
Joined: 8/3/2009 Last visit: 9/5/2025 Posts: 16343 Rating:
|
Hello mmkhan The basics for creating the project you can find here: https://support.industry.siemens.com/cs/de/en/view/89852595 Then also check if you have set the PGPC INterface settings in Windows Control Panel correctly that the accesspoint from the HMI connection in the HMI project is directed correctly to the correct networkcard If you still need help, which TIA Version do you use and which FW Version is your PLC using? Bye Murof |
Last edited by: Murof at: 07/02/2025 12:56:54If this Information really helps, you could use the Rate function |
|
Follow us on