(0)| 7/28/2025 10:26 AM | |
|
Joined: 8/6/2015 Last visit: 1/13/2026 Posts: 2 Rating:
|
I am experiencing same issues. I have a CPU 1517H and modbus redundand with CP 1543-1.
PLC is server and VIM is client.
If i try to connect with generic modbus client (modscan), everything works fine server side.
When i try to connect VIM i have unexpected behavior. If VIM can succesfully connect, whenever i try to switch the connection for redundancy test (unplug one of the 2 ethernet wire for modbus, or power off one of the siemens CPU) communication drop. After communication break there is no way to restore it in auto. I need to switch off and on again VIM, re-download config and pray to re-establish communication.
I am starting to think VIM is faulty or there is no compatibility between Siemens and Emerson VIM.
Was anyone out there succesfully integrate modbus Emerson VIM and S7-1500? ------------------------------------------------------------------------------------------ |
Last edited by: Wit_Moderator at: 07/29/2025 10:02:23New subject after splitting |
|
Follow us on