8/26/2025 10:34 AM | |
Joined: 8/22/2025 Last visit: 8/27/2025 Posts: 2 Rating:
|
Hi all,
We had a faulty SIMATIC HMI TP1500 Comfort in a plant and did a replacement. The originally installed model is 6AV2 124-0QC02-0AX1. However, only the one with prefix -0AX2 is available on site. We don't have the GSD file for the -0AX2 model, and from the release note (https://support.industry.siemens.com/cs/us/en/view/109817238), we were under the impression that the two are compatible for replacement. After replacing the faulty -0AX1 with the new -0AX2, the HMI is up and running with no issues reported by the operators. However, on HW config online diagnostic, the HMI's status is Module not available with the following message:
Any suggestion to clear the error? Many thanks in advance! ☺ |
8/27/2025 12:49 AM | |
Joined: 8/22/2025 Last visit: 8/27/2025 Posts: 2 Rating:
|
Hello, We're using TIA V17. The Topology View and Network View, as well as the error message is attached below. |
Follow us on