11/24/2006 8:02 PM | |
Joined: 9/1/2006 Last visit: 9/12/2025 Posts: 193 Rating:
|
Hi L-O, If it is S7-400 compatible Mitsubishi can probably supply youa sample or atleastinfo about the protocol that they use. I guess it doesn't support the S7-protocol directly. Most other vendors use simple ethernet communication that requires you to define a direct fetch and write connection port. That should be done in NETPRO. Then the panel can read/write to your variables. With some you need to load some special FC's. PS. It always good to collect all panel data in one datablock to speed things up (or one for receive and one for send data). I looked in this manualbut nothing aboutconnecting to Siemens.... i hope it is possible at all. Better contact the supplier for more info. Good luck. René |
12/4/2006 3:48 PM | |
Posts: 12 Rating:
|
Ok, i have contacted Bejers and asked them if they got a solution. Thanks for the help! L-O |
Follow us on