1/16/2006 9:48 AM | |
Posts: 14 Rating:
|
I have problem for loadingSimatic S7 V5.3 Software on The HP make laptop NX-6120 series.Please help. Sdd |
1/16/2006 11:09 AM | |
Joined: 9/1/2005 Last visit: 8/22/2025 Posts: 4114 Rating:
|
Hello Sdd, please give us more informations. Which kind of problems do you have? Are there special error messages or something like that? Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
1/22/2006 8:19 PM | |
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hi Sdd, This is a known problem with HP PC's. The HP PC is installed from a network and is not installed so that the things that have to throw away after a reboot could be throw away because they standing on a network drive that wasn't there anymore! I have hat the same trouble.... In the next link is discribed how to get this ok again: http://support.automation.siemens.com/WW/view/en/8861819 Please notice that this is no Problem of STEP7 but from HP PC!! [:mad:] Best regards, Late |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on