1/19/2016 9:31 AM | |
Joined: 6/4/2010 Last visit: 9/30/2024 Posts: 387 Rating:
|
Dear Rashid, You have to make sure that the settings on the Desigo Insight management station are done correctly and hat the baud rate corresponds with the baud rate of the NCRE controller. Please find attached the engineering manual with the necessary settings for the Desigo Insight NCRE connection. Please note that you have to install a direct link (0-modem) connection and to set the correct baud rate. Regarding your specific questions: Please note that this is quite a complex topic and it may be very difficult to get the system running without the detailed system information or a training. We therefore recommend to contact your local Siemens BT branch office or a Siemens representative to get support. Best regards, AttachmentCM110599en_DesigoInsight_Integral_Egineering.pdf (1229 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on