9/16/2008 11:18 AM | |
Joined: 8/31/2005 Last visit: 8/8/2025 Posts: 2198 Rating:
|
When I was working with SIMADYN D I had a serial cable that worked with SS1 and SS2. Ihr big advantage is you do not care, if there is a SS1 or SS2 pluged in, it will work anyway. I put the electonics in the 25 pin plug. The length of the cable should not ne longer than about 2m. For me it worked fine, but please note there is no galvanic isolation, so you may damage your PC/Notebook or the SIMADYN D rack. But as I said, for me it worked fine any time I used it. AttachmentV24-20mA.pdf (704 Downloads) |
|
|
Follow us on