8/2/2019 3:31 PM | |
Joined: 10/1/2013 Last visit: 9/10/2025 Posts: 605 Rating:
|
AFAIK there's no SCL example. But once you are familiar with SCL all those RFID applications will be even easier to implement (my opinion). I absolutely prefer SCL over all other languages. Especially the "IF..ELSE" system is very handy for handling async TIA blocks like those RFID blocks. Attached you'll find a small SCL example I wrote. Content:
I hope it helps a little. AttachmentRfidSCL_V15.1.zip (684 Downloads) |
This contribution was helpful to
1 thankful Users |
8/6/2019 12:31 PM | |
Joined: 10/1/2013 Last visit: 9/10/2025 Posts: 605 Rating:
|
Hi Carlos, error "16#E1FE_0200" just means that you moved the TAG out of the RF field while the operation was still running. I guess your block remains busy because you accidently start a new command. In real life I'd use a light barrier to trigger a command and not the presence indicator. "16#DF80_B000" is strange. This is a bus error. So there might be something wrong with your PROFINET connection. By the way, you'll find all the error codes here: |
This contribution was helpful to
1 thankful Users |
Follow us on