2/13/2020 1:54 AM | |
Posts: 19 Rating:
|
Hi expert's. My electrician wanted me to ask a question about the flat ribbon cable diagram SIM_RDY how much should there measure from that pin? |
2/14/2020 7:53 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Please refer SIMODRIVE 611 digital Drive Converters manual & attached sheet which explains timing diagram of activating terminals. HTH |
Last edited by: PISCEAN 2010 at: 02/14/2020 07:58:28Corrected timing diagram attached Last edited by: Jen_Moderator at: 02/14/2020 08:27:43Optimized link. |
|
2/26/2020 7:00 AM | |
Posts: 19 Rating:
|
Update, After days of testing drives 1 by 1 by disconnection the flat ribbon cable from the E/R module and letting it sit with power on for hours and reconnected the cables to see if it would function normally it took days of testing and found out X axis card was defect also the first card after NCU, we had and old defected LT-module that has the same type of control card, we put that in the X axis card and it booted up normally, but when I put control power on my C B axis makes sound on the machine and it has alarm 25050 I could move Y Z axis on the machine but X and C B I cannot, I will put back the original control card and let it sit to see if the error comes from the Y Z control card. ill keep you updated on what I find. (if power ON for 4 to 5 hours 300101 goes away and function normal) Attachmentpictures.zip (501 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on