3/4/2021 10:33 AM | |
Joined: 6/4/2010 Last visit: 9/30/2024 Posts: 387 Rating:
|
Dear Anony, It looks as the project has an Animated Gif in the graphic page (see AnimatedGif.png) based on the error message provided. Please try to find the graphic page where the animated gif is present and open the graphic page after enabling the trace channels (see CCtrace.png). It is recommended to process the trace with the standard CC client on the server. In case this is not possible, use the trace channels on the server and use the Clickonce. Afterwards please check the IIS log file (see IIS_LogFile, by default here C:\inetpub\logs\LogFiles) and PVSS_II.log in the project’s log folder. I hope that the trace information will help to identify the root cause. Otherwise you may contact you local customer support. Best regards, Albis AttachmentTraceAnimatedGif.docx (493 Downloads) |
This contribution was helpful to
2 thankful Users |
Follow us on