9/26/2014 6:26 PM | |
Posts: 2 Rating:
|
Please suggest me which parts I have to check for the Fault Code F026 in MasterDrive... |
9/26/2014 7:16 PM | |
Posts: 784 Rating:
|
Link1 ------- ------- ------- ------- ------- -------
|
9/27/2014 7:37 AM | |
Posts: 2 Rating:
|
Thanks for your reply... |
9/27/2014 10:51 PM | |
Posts: 93 Rating:
|
Dear sir first you have to check igbts for phase v replace faulty then u have to replace igd card finally you have to replace ivi dr alaa abozaid |
10/29/2014 6:52 AM | |
Posts: 5 Rating:
|
Hello, I have experience alot with this kind of Faults eg.F025,F026,F027respectively. As for your reference these faults: F025=UCE Ph. L1 A UCE shutdown has occurred inphase L1 F026=UCE Ph. L2 A UCE shutdown has occurred inphase L2 F027=UCE Ph. L3 A UCE shutdown has occurred inphase L3 Now, for your remedy with these faults you must directly replaced theIGD-Inverter Gate Driveboard with respect to the location of the fault. Example: if the fault isF025, then replaceIGDboard inPhase Line 1. if the fault isF026, then replaceIGDboard inPhase Line 2. if the fault isF027, then replaceIGDboard inPhase Line 3. But before you conclude that its theIGD boardis defective please check first the connection of allFIBER OPTIC ![]() ![]() Cheers, MikeCarts |
10/30/2014 3:24 PM | |
Posts: 93 Rating:
|
dear friend you have to check the following and replace if faulty 1- igbt phase v 2- igd phase v finally ivi
|
2/20/2023 8:59 AM | |
Joined: 12/14/2022 Last visit: 2/23/2023 Posts: 2 Rating:
|
Can you please explain what are you doing with resistors in your photo? Thanks Best regards Miguel |