3/22/2025 8:36 AM | |
Joined: 10/21/2024 Last visit: 7/17/2025 Posts: 13 Rating:
|
Sounds right. But than should my program work or can you find any other mistake? |
3/22/2025 10:36 AM | |
Joined: 12/18/2014 Last visit: 9/16/2025 Posts: 35964 Rating:
|
Possibly an overlap in the VM memory due to double allocation of VW0? |
3/23/2025 7:41 AM | |
Joined: 12/18/2014 Last visit: 9/16/2025 Posts: 35964 Rating:
|
@ AutoGen_97368, I have make a test with a LOGO! 8.FS4 and a modbus server simulation program. See attached screen video. AttachmentScreencast 2025-03-23 08-37-15.avi (319 Downloads) |
This contribution was helpful to
1 thankful Users |
3/24/2025 8:06 AM | |
Joined: 10/21/2024 Last visit: 7/17/2025 Posts: 13 Rating:
|
Here is my program. I belive something is wrong with VW addresses. See next post.
AttachmentModbustest.zip (201 Downloads) |
3/24/2025 8:28 AM | |
Joined: 12/18/2014 Last visit: 9/16/2025 Posts: 35964 Rating:
|
In the Modbus connection table have the entries: VW0 - 2 Words - HR1 - 2 Words With the first entry writes write you VW0 and VW2 to HR1 and HR2. An Holding Register is a Word (16 Bit). But the addressing of HR and VW are different. Example: HR1, HR2, HR3, HR4 and so on ... AttachmentLOGO! Bit, Byte, Word and DWord.pdf (266 Downloads) |
3/24/2025 9:06 AM | |
Joined: 10/21/2024 Last visit: 7/17/2025 Posts: 13 Rating:
|
Thats the configuration of the modbus relais. |
3/24/2025 11:29 AM | |
Joined: 12/18/2014 Last visit: 9/16/2025 Posts: 35964 Rating:
|
Can you show me a screenshot of the Modbus Poll when you switching on the relay? |
3/24/2025 11:41 AM | |
Joined: 12/18/2014 Last visit: 9/16/2025 Posts: 35964 Rating:
|
Try this ... |
This contribution was helpful to
2 thankful Users |
3/24/2025 1:21 PM | |
Joined: 12/18/2014 Last visit: 9/16/2025 Posts: 35964 Rating:
|
That sounds good ... |
Follow us on