(0)| 3/24/2025 12:33 PM | |
|
Joined: 7/11/2024 Last visit: 12/30/2025 Posts: 200 Rating:
|
Hello bercow, The first option (using memory addresses directly in the program) I would not recommend unless your program is very, very simple. As the program grows, it will be very difficult to work directly with memory addresses. Creating a variable for each I/O and putting them in a single data block would improve code readability and facilitate debugging compared to the previous option. However, I recommend you to use more DBs to to better organize the code. In the third approach the program calls the Function Blocks to interact with the I/O, rather than directly referencing the physical addresses. This is a good option when you need to perform the same actions in diffenrent parts of your code. Also, it improves code understanding and makes debugging easier. Finally, UDTs (User Defined Types) are useful to group related input and output signals. They also improve code reusability, understanding and debugging. The choice depends on the requirements of the project, how complex is it and the programmer personal preferences. Usually, the more modular and abstracted the I/O handling is, the easier it is to maintain and modify the program in the long run. Check:Basics of PLC data types (UDT, Function blocks (FB) and Basic principles for programming of data blocks |
|
If this post has been useful, don't forget to rate it!😊 |
|
This contribution was helpful to
|
|
Follow us on