2/3/2025 7:11 AM | |
Joined: 3/14/2008 Last visit: 9/17/2025 Posts: 2217 Rating:
|
Hi, See the following manual chapter 5.2.7 for more information about the behaviour: CFC readme Basically it is the same. Instead of using I/O in the SFC, you can use sort of a placeholder like SetOpen. In SetOpen you can use the SFC logic like Initialization/Processing/Termination. So you can decide how to use the technological action. With If-then-else statements, it works a bit different as you can see in the manual. |
Last edited by: Moderator_Lan at: 02/03/2025 09:13:49link optimized If I could help you, you can use the RATE button. Thank you. |
|
Follow us on