(0)| 9/27/2024 12:17 PM | |
|
Joined: 10/17/2023 Last visit: 12/6/2024 Posts: 10 Rating:
|
Dear Forum Members, Version: Unified V19 Browser: Chrome Goal: start simulation --- Errors in TraceViewer: Project validation failed! Detected high level error (for details see following info traces): The runtime is running, operation expects stopped runtime (22) Attempted to stop runtime, while there's still another service created! CC_EventHandler::disconnect: current state for disconnect: %d %d %d %d %d [0, 0, 0, 1, 0] Precondition 'CheckLanguage(filterLang)' failed! (Hmi::QF::ActiveAlarmSubscriptionHandler::Subscribe) dai is NULL Unexpected state, CReadCallback, handle_result, error -9204590179157540888 Cid=,318 Oid=, 0x2 CHmiRuntime::Could not start project - project name missing in CContextStore! --- Result: simulation running but "site cannot be reached ... ERR_CONNECTION_RESET" Attempts but same error:
Where is the CHmiRuntime folder? Sounds something is wrong there. I assume it's C:\ProgramData\SCADAProjects but not sure How do you properly "rebuild runtime/project"? Maybe unrelated but connecting to WinCC SQL server through SSMS also showed no file. Did I miss some configuration? What else can be done |
| 9/30/2024 3:28 PM | |
|
Joined: 10/17/2023 Last visit: 12/6/2024 Posts: 10 Rating:
|
Dear MindFlayer, After punching the air through the weekend, we finally hit the ghost: Settings for communication with WinCC Unified Runtime on the runtime device Turns out the user was not a member of SIMATIC HMI VIEWER group. Click Add... > Type what is missing under "Enter the object names to select" field. Then adjust everything in WinCC Unified Configuration as described in the link above. --- Note for Windows 11: Instead of "Administrative Tool", go to Control Panel > Windows Tool > Computer Management > System Tools > Local Users and Groups Note in general: after googling an error, try the "More results from support.industry.siemens.com" link. Sometimes good answers and links are already discussed in the Forum but not visible on the first page of google search. |
This contribution was helpful to
|
|
Follow us on