9/4/2024 10:15 AM | |
Joined: 5/18/2023 Last visit: 10/16/2024 Posts: 1 Rating: (0) |
Hello We have a S120-CU320PN_2 with 2 axis and want to read the parameters with Node-Red. I have attached a picture with the different parameters. Is it possible to read the values from the moduls? How can the same R parameters be addressed on the different modules? Module 2 is for axis Z11 and Modul 3 is for axis Z12. Which adresses do I need for the different moduls? Many thanks in Advance. BR M. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 09/04/2024 10:32:37New subject after splitting |
|
Follow us on