12/7/2021 8:15 AM | |
Joined: 4/29/2021 Last visit: 12/28/2021 Posts: 50 Rating: (0) |
Dear Experts, We have purchased both DCM Drive . I have enclosed here for DCM drive name plate . Pls remove txt in my attachment find the image on the drive rar file name plate...... Pls confirm this both drive having inbuild Profinet communication . Thanks In advance, Regards, AttachmentDCM Drive Manual.rar.txt (592 Downloads) |
12/7/2021 9:15 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (878)
|
Hello, Could not open attachment. Why don't you combine snap shot of nameplate files in zip folder & attach? |
12/7/2021 9:27 AM | |
Joined: 12/18/2014 Last visit: 11/11/2024 Posts: 34190 Rating: (4260) |
Here's the same as ZIP file ...
AttachmentDCM Drive Manual.zip (595 Downloads) |
This contribution was helpful to2 thankful Users |
12/7/2021 9:50 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (878)
|
Hello Puli Kutty, 6RA8018-6DV62-0AA0 is basic 4Q 25A DC drive. 6RA8031-6DV62-0AA0 is basic 4Q 125 A DC drive. To connect Profinet, user need to go for advanced CUD unit + profinet module which is option. Please check the convenient location of installation of advanced CUD in drive & then user can order left or right advanced CUD along with Profinet board. Hope this helps. |
Follow us on