12/15/2021 10:16 PM | |
Posts: 257 Rating: (79)
|
Hello SIOS Forum Community Here is a hint that should serve as a rough guide if you are about to decide to change the hardware from S7-300/S7-400/ET 200S to S7-1500/ET 200SP. When selecting the new hardware, a CM or CP may have to be extended depending on the requirements if PROFINET or Profibus or other is not already integrated in the controller. Assignment SIMATIC S7-300👉SIMATIC S7-1500 CPU S7-312/S7-314👉CPU S7-1511-1PN CPU S7-315-2DP (DP-SS with CM/CP)👉CPU S7-1513-1PN CPU S7-315-2PN/DP (DP-SS with CM/CP)👉CPU S7-1515-2PN CPU S7-317-2DP + S7-317-2PN/DP👉CPU S7-1516-3PN/DP CPU S7-319-3PN/DP👉CPU S7-1517-3PN/DP CPU S7-319-3PN/DP👉CPU S7-1518-4PN/DP Assignment SIMATIC S7-400👉SIMATIC S7-1500 CPU S7-412-1👉CPU S7-1513-1PN CPU S7-412-2👉CPU S7-1515-2PN CPU S7-412-2PN + S7-414-2PN👉CPU S7-1516-3PN/DP CPU S7-414-3👉CPU S7-1517-3PN/DP CPU S7-414-3PN/DP + S7-416-2👉CPU S7-1518-4PN/DP Assignment SIMATIC ET200S👉SIMATIC S7-1500/ET200SP CPU S7- ET200S IN 151-7👉CPU S7-1510SP-1PN CPU S7- ET200S IN 151-7 FO👉CPU S7-1510SP-1PN CPU S7- ET200S IN 151-8 FO👉CPU S7-1512SP-1PN Supplementary further information: SIMATIC S7-1200 / S7-1500 Comparison list for programming languages Short explanation of the abbreviations chosen above if not known: DP: Profibus PN: PROFINET CP: Communication Processor CM: Communication Module IM: Interface Module FO: Fibre Optic Connection SS: Interface Best regards, SIMATIC International Technical Support Hub |
This contribution was helpful to1 thankful Users |
Follow us on