6/24/2020 10:10 PM | |
Joined: 9/16/2013 Last visit: 1/5/2024 Posts: 511 Rating:
|
Just to inform the community with the problem in Unified V16 update 1 with establishing modbus TCP connection(Projects could not be downloaded after selecting Standard Modbus TCP/IP as a HMI connection) that has been approved and resolved as well in damn short time by Siemens: Message on May 28, 2020 "I tested the behavior with a new project on our WinCC Unified V16 update 1 system and I could reproduce the behavior. And good news on 18 June 2020 "I uploaded a setup package to the FileShare. After installing it, the issue should be gone. The package will also be available on SIOS shortly." Best Regards Soble |
Last edited by: SOble at: 06/24/2020 22:11:11Last edited by: SOble at: 06/24/2020 22:15:37Website: |
|
This contribution was helpful to
2 thankful Users |
4/30/2022 5:19 PM | |
Joined: 11/7/2008 Last visit: 12/19/2022 Posts: 9 Rating:
|
Hi, the link you posted is not accessible. Do you have another way to post this patch please? Many thanks |
Follow us on