8/16/2022 8:46 AM | |
Joined: 4/8/2021 Last visit: 6/17/2024 Posts: 638 Rating:
|
Hi Abdullah1, Regarding your 2 first questions, to my knowledge KTP Basic Panels can't be integrated in your Simatic Manager project, therefore, you must configure it using TIA Portal. In addition, there should be no problem to establish the communication between the PLC and the panel if both are not configured with the same software. Regarding your PROFIBUS segment length, AFAIK 100m is supported and you can use the following speed transmision https://support.industry.siemens.com/cs/ww/en/view/15115523 Finally, i'm not sure what do you mean by "continuous" communication. Hope it helps. Br, Cocolino |
Best regards, |
|
8/19/2022 8:28 AM | |
Joined: 4/8/2021 Last visit: 6/17/2024 Posts: 638 Rating:
|
Hi Abdullah, Have a look a this FAQ I think it explain the same application case as yours. https://support.industry.siemens.com/cs/ww/en/view/73502293 Br, |
Best regards, |
|
Follow us on