9/7/2022 9:30 AM | |
Joined: 4/22/2020 Last visit: 8/10/2024 Posts: 4 Rating: (1) |
Hello dear I am setting up a Fritz Werner TC630 With Sinumerik 850m, Machine Number 816480, but I don't have the basic parameters. After loading the parameters of NC MD, PLC MD, one of the machines that is similar to this machine and is in the attached file, all the axes go to reference except Magazine and the spindle does not rotate with the handwheel. It is necessary to explain that there are 6 similar devices with Sinumerik 850&880 controls and they are working. Help me please. ------------------------------------------------------------------------------------------ AttachmentTc630.zip (346 Downloads) |
Last edited by: Jen_Moderator at: 09/21/2022 10:07:02New subject after splitting |
|
9/7/2022 9:42 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877)
|
Hello Hadi0291, You have posted your same problem/issue/query in numerous old topics, of which, most members are not present in forum. Instead of opening multiple topics, please open new topic for your query & wait. Members/experts who are much familiar with old system e.g. nulizhang or Pee El Sea etc. etc. might reply you. Hope this helps. |
9/21/2022 10:08 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subjectSiemens 850M controlled TC630 machine recovery problem is published within the conference SINUMERIK CNC automation systems. Jen_Moderator |
Follow us on