8/1/2022 1:40 PM | |
Posts: 71 Rating:
|
Hello Duccio, When using multimonitor, the main monitor must be always set on the upper left corner. If your OS has 4 monitors, (from left to right: 1-2-3-4) and for example your main monitor is monitor number 3, change the main screen from monitor 3 to monitor 1. This should solve your problem and you should see the login interface in that monitor. You can check more detailed information about this in the following link: - Notes on Multi VGA https://support.industry.siemens.com/cs/ww/en/view/109762744/81976355339 Best regards, s7-mencey. PD: If this post helped you, don't forget to rate with 5 stars! |
This contribution was helpful to
1 thankful Users |
Follow us on