10/6/2022 2:05 AM | |
Joined: 1/16/2015 Last visit: 4/18/2024 Posts: 46 Rating: (1) |
Hello, I am facing that same problem now, which is that Accessible nodes doesn't work with any of Siemens products (TIA portal, Step7, Scout,...) but if i configure the device with a predefined IP, i can connect to it without problem with all of the programs above. I tried a wireshark capture during the Accessible node, and i found that the PC sends two LLC requests, and the none of the devices responds to it... I am wondering what could be goind wrong? is the LLC protocol the right one for accessible nodes? and if yes, why none of the nodes is responding, and therefore is not detected by the program? Below is a screenshot of the wireshark capture for the request Thanks for your help Best regards Phil ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/06/2022 07:23:01New subject after splitting Last edited by: Jen_Moderator at: 10/11/2022 06:27:19Spelling mistake in the headline optimized. |
|
Follow us on