10/6/2022 12:27 PM | |
Joined: 11/13/2017 Last visit: 1/19/2024 Posts: 1 Rating: (0) |
Dear Expert, I am using 6ES7 153-1AA03-0XB0 modules in GE-Fanuc Software (Proficy machine edition 7.5). The hardware for PLC is PC based SST-PB3-PCU card, molex made. I have tried all 3 GSD file which is on website mentioned above thread. But PLC is not communicating with IM153-1 and in profibus Network status it is giving error code 2049 (Mean Bus config error, usually in GE it shows that your added I/O modules has different configuration than added in software) Following I/O slave added in configuration- 1. DO 32- 6ES7322-1BL00-0AA0 2. DI-16 6ES7 321-1BH02-0AA0 3. AI 8- 6ES7 331-7NF00-0AB0 4. AO8- 6ES7 332-5HF00-0AB0 Please help me with, I doubt on GSD file or is this specific IM153-1 model is able to handle I/O mentioned on top? may be some firmware issue?? awaiting your valuable comment. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/07/2022 06:57:27New subject after splitting |
|
Follow us on